AXIS#.MOTOR.PHASE

Description

This parameter is the relative alignment of the feedback to the motor coils. For Kollmorgen motors, the feedback and coils are aligned, and AXIS#.MOTOR.PHASE may be set to 0.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Electrical degrees

Range

0 to 360
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
AXIS1.MOTOR.PHASE

500bh

15h

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.PHASE

510bh

15h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.PHASE

6210

1842

Unsigned16

Read Only

-

AXIS2.MOTOR.PHASE

71746

1184

Unsigned16

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.PHASE

6210

Unsigned16

Read Only

-